Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Hello,
I have two questions here.
1. I want to design hardware interface between CLB unit and external encoder, the encoder is with Endat, Biss or the RS485 based prototype. Is TI provided any reference documents related them?
2. I want to realize the EtherCat communication on tms320f280049C chip, I have learned that can be implemented using FSI port on 280049C, which may be possibly achieved higher bode rate than other peripheries on the 280049C. But currently I have no idea how to design such hardware interface, for example, how to connect between 280049c and external Ethercat chip. Is TI provided such reference document?
Any help will be appreciated.