This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: RDK3.1 DRV8320rs symbols

Guru 56418 points

Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: DRV8320

Hello,

Oddly CCS complains of missing symbols building RDK3.1 eabi projects when they are clearly instantiated in the index. It seems related to define DRV8320_SPI being removed then add back into any of the lab projects.

Oddly the same 3 basic calls exist in drv8320.h but have been deemed external functions in hal.h and renamed to add to the confusion. Why are these 3 functions first declared drv8320.h being called from hal.h under a alias name seems to be part of the issue. What is causing both RDK v2.1 and v3.1 to have these same 3 missing symbols?