This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Failed booting from Flash after reset the DSP for the example program TIDM-2008 provided by TI

Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMDSCNCD280049C, SFRA

Short description: Not booting from flash

I am using TMDSCNCD280049C to check your existing example solution TIDM-2008. I have successfully loaded the program into Flash memory. But when I reset the device, the program is not booting from flash. It is running initially, after I reset the device the boot from Flash failed.  I have attached here the CCS window, the program has stopped at the address 3FB02A as shown in the image.