Part Number: TMS320F28076
Other Parts Discussed in Thread: UNIFLASH
Dear support,
First of all: A hardware test version is equipped (TMS320F28076 with everything necessary).
The CCS has accepted my 2807x_eigener_lnk.cmd.
With the XDS100V3 I was able to load, start and debug the program with the CCSV9.3 and 10.2 in the RAM
and it runs correctly (2807x_eigener_lnk.cmd == content of 2807x_Generic_RAM_lnk.cmd)
Then I exchanged the content of 2807x_eigener_lnk.cmd for 2807x_Generic_FLASH_lnk.cmd and tried to load the program into the FLASH.
Now I get the following error message:
C28xx_CPU1: GEL Output: Memory Map Initialization Complete C28xx_CPU1: Flash Programmer: The calculated system clocks (190.00) is not within the valid range for this device [0.00,120.00]. C28xx_CPU1: File Loader: Memory write failed: Unknown error C28xx_CPU1: GEL: File: D: \ CCSV9.3 \ CODE_28076 \ FRD_TEST_IOs \ CPU1_FLASH \ FRD_TEST_IOs.out: Load failed.
I get this error message from the CCSV9.3, CCSV10.2 and the UNIFLASH.
First question: Where are the system clocks set to 190.00?
Second question: Where and how do I have to set the system clock so that the error is corrected?
Third question: How and where does the CCS recognize that the FLASH_PROGAMM has to be called or that data are only to be transported to RAM.
With kind regards
Friedrich