This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: Flash Kernel Problems

Part Number: TMS320F28375D

I have been using the flash-kernel (default files) to program the device. However, when I do DFU1 it gives me the following error:-
SUCCESS of Command
ERROR Status: VERIFY_ERROR
ERROR Address: 0x80000

Even though the application load is successful.

But, when I DFU2, it fails with the following error:-


Checksum does not match... Please press Ctrl-C to abort.

This is coming from the following code:- 


void loadProgram_checksum(FILE *fh)

....

//Send ACK as expected
WriteFile(file, (unsigned char*)&ack, 1, &dwWritten, NULL);

rcvData = (sendData[1] << 8) + sendData[0];

//Ensure checksum matches
if (checksum != rcvData)
{
printf("\nChecksum does not match... Please press Ctrl-C to abort.");
 while (1){}
}

while (fileStatus == 1)
{
unsigned int blockSize;

This happens all the time. This works with the blinky apps and our older .hex files. However, it fails consistently with our newer hex files. I have attached the linker files. I can send the .map files as well.

Please let me know if any additional information is required.


CPU1 


MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */

PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 :

BOOT_RSVD : origin = 0x000002, length = 0x00007E /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800


RAMLS5 : origin = 0x00A800, length = 0x000800

RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x00B000
RAMGS12131415 : origin = 0x018000, length = 0x003FF8 // For cpu2
// RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */

CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400

}

SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(8)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(8)
codestart : > BEGIN PAGE = 0, ALIGN(8)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.switch : > FLASHB PAGE = 0, ALIGN(8)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

#if defined(__TI_EABI__)
.init_array : > FLASHB, PAGE = 0, ALIGN(8)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS3, PAGE = 0 ALIGN(8)
.bss:cio : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.const : > FLASHF, PAGE = 0, ALIGN(8)
#else
.pinit : > FLASHB, PAGE = 0, ALIGN(8)
.ebss : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
.cio : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHF PAGE = 0, ALIGN(8)
#endif

#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif

#endif

/*** User Defined Sections ***/
FWVERSION_MEM : > RAMGS0, PAGE = 1
CONFIG_AIM_MEM : > RAMGS0, PAGE = 1
CALIBRATION_AIM_MEM : > RAMGS0, PAGE = 1
ACK_MSG_CONFIG_MEM : > RAMGS0, PAGE = 1
ACK_MSG_CALIBRATION_MEM : > RAMGS0, PAGE = 1

RMS_HALF_MEM : > RAMGS1, PAGE = 1
EVENTS_FIFO_BUFFER_MEM : > RAMGS1, PAGE = 1
TRENDS_FIFO_BUFFER_MEM : > RAMGS1, PAGE = 1
BUFFERS_MEM : > RAMGS1, PAGE = 1


/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

CPU2


MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000080, length = 0x000380
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800

RAMLS5 : origin = 0x00A800, length = 0x000800

RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x00B000
RAMGS12131415 : origin = 0x018000, length = 0x003FF8 // For cpu2
// RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */

CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}


SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(8)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(8)
codestart : > BEGIN PAGE = 0, ALIGN(8)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.switch : > FLASHB PAGE = 0, ALIGN(8)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

#if defined(__TI_EABI__)
.init_array : > FLASHB, PAGE = 0, ALIGN(8)
.bss : > RAMLS5, PAGE = 1
.bss:output : > RAMLS3, PAGE = 0 ALIGN(8)
.bss:cio : > RAMLS5, PAGE = 1
.data : > RAMLS5, PAGE = 1
.sysmem : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.const : > FLASHF, PAGE = 0, ALIGN(8)
#else
.pinit : > FLASHB, PAGE = 0, ALIGN(8)
.ebss : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
.cio : > RAMLS5, PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHF PAGE = 0, ALIGN(8)
#endif

#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif

#endif

/*** User Defined Sections ***/
COMM_RX_BUFFER_MEM : > CPU2TOCPU1RAM, PAGE = 1
SDP_CONTEXT_MEM : > RAMGS12131415, PAGE = 1

/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}

GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}


/*
//===========================================================================
// End of file.
//===========================================================================
*/