Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE,
Greetings,
I am using CCS 9.1.0.00010, and have a project in which the Target Configuration has been setup to use our normal GEL files which I have confirmed are in the correct folder. But when I try to debug the project, I get the error messages below. There are other messages, but I believe they have resulted because our GEL files are not seen by the launch. Is there something else which should be setup?
C28xx_CPU1: GEL: Error loading file 'C:\ti\ccs910\ccs\GelFiles\f28379d_cpu1.gel': unable to open GEL file 'C:\ti\ccs910\ccs\GelFiles\f28379d_cpu1.gel'
C28xx_CPU2: GEL: Error loading file 'C:\ti\ccs910\ccs\GelFiles\f28379d_cpu2.gel': unable to open GEL file 'C:\ti\ccs910\ccs\GelFiles\f28379d_cpu2.gel'
Thank you,
Ed