Part Number: TMS320F28388D
Hi,
I use ecap module to measure motor speed with ecap 5 module.
I configure the register settings with respect to my application.
PIE interrupts and ecap 5 interrupt is enabled and global interrupt bit INT is 0, clock and CPU selections are configured before.
The interrupt occurs on ECEINT.bit.CEVT4 but the corresponding flag bit is not set(ECFLG.bit.CEVT4) so the capture registers CAP1, CAP2, CAP3, CAP4 reads 0.
Why that happens so ?
Does overflow affect the above functionality?
Thanks,
Subha