Part Number: TMS320F28027
Other Parts Discussed in Thread: TPS3306
Hello.
As shown in the attached circuit diagram, there is a circuit configuration of TMS320F28027 and external WD (TPS3306).
When rewriting the program with JTAG, open the jumper and disable the external WD.
But sometimes I forget to open it and do it closed.
In this case, the reset will be applied during writing and the writing will fail.
Also, the CPU will not be able to connect to JTAG and will never be usable again.
Do I get the same result when using SCI_BOOT?
Is there any countermeasure with SW / HW that does not damage the CPU even if I make the above mistake?
Thanking you in advance.