Other Parts Discussed in Thread: TMS320F28335
Hi
I am trying to store data from a buffer on the RAM to the a buffer on flash memory, but i can't make it work.
When i inspect the memory from CCSv4 it seems like the flash memory somehow is write protected. (Memory Protection Flags: [Write Protected]).
The flash memory is defined in as:
Memory(page 1):
FLASHA : origin = 0x300000, length = 0x008000
Section
.toFLASHA : > FLASHA, PAGE = 1
In the main file we use:
================
// Variable for data collection
#pragma DATA_SECTION(Table, ".toFLASHA"); // Put data from Table into Flash
unsigned short Table[x]; // Table for datacollection with x entrances
===============
Is it possible to change the flag value, and how?
The reason why we want to use the flash memory is because the RAM doesn't contain sufficient space.
I am using the Delfino TMS320F28335.