In the TRM for F2838x and F28002x, it is mentioned that the structure of CLB Input X-bar and CLB Output X-bar is that of Input X-Bar and Output X-bar respectively. Does this mean that the register names are also exactly same?
We can refer to registers like ClbOutputXbarRegs.OUTPUT1MUX0TO15CFG or ClbInputXbarRegs.INPUT1SELECT and so on?
Also for CLB Output X-BAR MUX16-31 are reserved, do we still have OUTPUT#MUX16TO31CFG register for CLB Outputs?