This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: SPIA on F2800025

Part Number: TMS320F280025

Hi,

Good day.

Our customer has a problem on the SPIA of the TMS320F280025. Kindly see below for their description.

"I'm having a problem with SPIA on F280025A device
It only works if I use GPIO16=SPISIMOA;  GPIO17=SPISOMIA;  GPIO18=SPICLKA;  GPIO19=SPISTEA
If I configure GPIO1=SPIAMISO it doe not work

I'm using the sample code spi_exe1_loopback in TI dev board
if I configure SPI in loopback mode works fine
then I changed to normal mode, made wire jumper GPIO16 and GPIO17 and works good as well

now if I configure GPIO1 as SPIAMISO the SPI does not works"

We appreciate your help on this matter. Thank you.


Regards,

Cedrick