Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi, sir.
I'm using tms320f28388D custom board.
I have been implementing DFU using external flash memory integrated in my custom board.
Currently, I stored and read the CPU1 boot image using SPI communication from external flash memory and successfully booted from CPU1.
In the same way, I try to store and read CPU2 image from external flash memory in the CPU2 using SPI.
So I set it up like this:
---------------------------------------------------------------------------------------------------------------------------------
[CPU1]
Device_init();
Device_initGPIO();
//GPIO setting
GPIO_setPinConfig(GPIO_16_GPIO16);//GPIO16 -> FLASH_WP
GPIO_setPinConfig(GPIO_57_GPIO57);//GPIO57 -> FLASH_CS
GPIO_setPinConfig(GPIO_54_SPIA_SIMO);-> FLASH_SIMO
GPIO_setPinConfig(GPIO_55_SPIA_SOMI);-> FLASH_SOMI
GPIO_setPinConfig(GPIO_56_SPIA_CLK);-> FLASH_CLK
GPIO_setDirectionMode(FLASH_WP, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(FLASH_WP, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(FLASH_WP, GPIO_QUAL_SYNC);
GPIO_setDirectionMode(FLASH_CS, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(FLASH_CS, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(FLASH_CS, GPIO_QUAL_SYNC);
GPIO_setDirectionMode(100, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(100, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(100, GPIO_QUAL_SYNC);
GPIO_setMasterCore(16, GPIO_CORE_CPU2);//WP
GPIO_setMasterCore(57, GPIO_CORE_CPU2);//CS
GPIO_setMasterCore(54, GPIO_CORE_CPU2);//SIMO
GPIO_setMasterCore(55, GPIO_CORE_CPU2);//SOMI
GPIO_setMasterCore(56, GPIO_CORE_CPU2);//CLK
GPIO_setMasterCore(100, GPIO_CORE_CPU2);//CPU2 boot check gpio
GPIO_writePin(FLASH_WP, 1);//HIGH
GPIO_writePin(FLASH_CS, 1);//HIGH
//SPI setting
SysCtl_selectCPUForPeripheral(SYSCTL_CPUSEL6_SPI, 1, SYSCTL_CPUSEL_CPU2);
SPI_disableModule(SPIA_BASE);
SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA1, SPI_MODE_MASTER, 1000000, 8);
SPI_disableFIFO(SPIA_BASE);
SPI_disableLoopback(SPIA_BASE);
SPI_setEmulationMode(SPIA_BASE, SPI_EMULATION_STOP_MIDWAY);
SPI_enableModule(SPIA_BASE);
// Boot to CPU2
Device_bootCPU2(BOOTMODE_BOOT_TO_FLASH_SECTOR0);
//CPU2 check
while(GPIO_readPin(100) == 0);
while(1)
{
...
}
[CPU2]
Device_init();
CS_LOW;
SPI_writeDataBlockingNonFIFO(SPIA_BASE, WREN);
SPI_readDataBlockingNonFIFO(SPIA_BASE); -> stopped.
CS_HIGH;
GPIO_writePin(100,1);
while(1)
{
...
}
---------------------------------------------------------------------------------------------------------------------------------
The problem is that the GPIO setting is fine, but it freezes when getting data using SPI communication from CPU2.
I wonder what I was wrong. There seemed to be no way of using CPU2's SPI in TRM or c2000ware.
Could I use SPI on CPU2? If so, How should I configure the SPI?
Thank you.