Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Hello,
I have upgraded my computer and deciced (maybe not a wise decision...) to upgrade my project to the new tools provided by TI.
My old tools where: CCS v7.4.0.00015 Compiler v16.9.4.LTS C2000Ware 1.00.3.00
The new set of tools is: CCS v10.2.0.00009 Compiler v20.2.4.LTS C2000Ware 3.4.0.00
I started by creating an "empty project with main.c" and replaces with my main.cpp and added all my .cpp and .h files.
After adding the relevant "includes" in the "C2000 Compiler" -> "Include Options" section, I got my project to compile.
I am using XDS100V2 as my debug probe.
Now the project compiles and runs while the debugger is connected.
However, after a power cycle, the software dose not run.
Pasted below is the linker file.
Please help
Thanks
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
FLASHO : origin = 0x0C0000, length = 0x002000 /* on-chip Flash */
FLASHP : origin = 0x0C2000, length = 0x002000 /* on-chip Flash */
FLASHQ : origin = 0x0C4000, length = 0x002000 /* on-chip Flash */
FLASHR : origin = 0x0C6000, length = 0x002000 /* on-chip Flash */
FLASHS : origin = 0x0C8000, length = 0x008000 /* on-chip Flash */
FLASHT : origin = 0x0D0000, length = 0x008000 /* on-chip Flash */
FLASHU : origin = 0x0D8000, length = 0x008000 /* on-chip Flash */
FLASHV : origin = 0x0E0000, length = 0x008000 /* on-chip Flash */
FLASHW : origin = 0x0E8000, length = 0x008000 /* on-chip Flash */
FLASHX : origin = 0x0F0000, length = 0x008000 /* on-chip Flash */
FLASHY : origin = 0x0F8000, length = 0x002000 /* on-chip Flash */
FLASHZ : origin = 0x0FA000, length = 0x002000 /* on-chip Flash */
FLASHAA : origin = 0x0FC000, length = 0x002000 /* on-chip Flash */
FLASHAB : origin = 0x0FE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/