Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: ISO7741
Hi ~I want to ask some question for LaunchPad28379 Board
First, I want to use Ecap module in LaunchPad28379.So my signal input through J11
The circuit as picture below.I also use IC ISO7741. And IC output should be 5V pulse wave.
And connect 51ohm and 1nF to J11

I don't know why need 1K ohm and 1nF in board(as second picture shows)??
If consider 1k ohm and 1nF in board.How can I calculate RC time constant for my pulse wave which ISO 7741 output?
And also I want to know how does dsp can determine waveform rising and falling edge for Ecap?