Other Parts Discussed in Thread: UNIFLASH
Hi expert,
My customer need to use uniflash to program the device returned from factory.
and they need to program code with DCSM.
however, they told me they can finish it.
I did the test in my labtop using TI launchpad.
my uniflash version is
and i can program code without DCSM successfully.
but can not program code with DCSM.
after that, I program the DCSM code by CCS to verify the code is normal, and then I can see the password changed.
so i want to know why the code with DCSM can not be programmed.
it showed errors as below:
[2021/3/23 下午1:45:14] [ERROR] C28xx_CPU1: Error during Flash Programming. Address 0x00078000, Data 0x0000E000, FMSTAT 0x00000030
[2021/3/23 下午1:45:14] [ERROR] C28xx_CPU1: File Loader: Memory write failed: Unknown error
[2021/3/23 下午1:45:14] [ERROR] C28xx_CPU1: Error during Flash Programming. Address 0x00078004, Data 0x0000E000, FMSTAT 0x00000030
[2021/3/23 下午1:45:14] [ERROR] C28xx_CPU1: Please make sure the memory location you are programming have not already been programmed.
BR
Emma