Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Dear E2E Support Expert,
We are using TMS320F28388D for EtherCAT communication.
When using the debugger, the PHY Clock is output at 25Mhz according to the settings below.
But when I do not use the debugger and use it as FLASH memory, it often outputs 50Mhz and I can't do EtherCAT communication.
Thanks and Best Regards,
HJ.
main()
{
...
Device_bootCPU2(BOOTMODE_BOOT_TO_FLASH);
configureAndReleaseCMToWait();
SysCtl_setECatClk(SYSCTL_ECATCLKOUT_DIV_2, SYSCTL_SOURCE_SYSPLL, ESC_USE_INT_PHY_CLK); //PLLSYSCLK = 200MHz, ECatCLK = 100MHz
releaseCMToApplication();
...
}
configureAndReleaseCMToWait(void)
{
SysCtl_setCMClk(SYSCTL_CMCLKOUT_DIV_1, SYSCTL_SOURCE_AUXPLL); //AUXPLLCLK = 120MHz, CMCLK = 120MHz
IPC_setBootMode(IPC_CPU1_L_CM_R, (BOOT_KEY | CM_BOOT_FREQ_120MHZ | BOOTMODE_BOOT_TO_WAIT));
IPC_setFlagLtoR(IPC_CPU1_L_CM_R, IPC_FLAG0);
SysCtl_controlCMReset(SYSCTL_CORE_DEACTIVE);
}
releaseCMToApplication(void)
{
IPC_setBootMode(IPC_CPU1_L_CM_R, (BOOT_KEY | CM_BOOT_FREQ_120MHZ | BOOTMODE_BOOT_TO_FLASH));
IPC_setFlagLtoR(IPC_CPU1_L_CM_R, IPC_FLAG0);
}