Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE
-
GPIO 28/29 is configured as SCIA
-
To enter in the boot loader mode, during reset, GPIO24 is low and GPIO32 is high
-
I'm sure the MCU is in boot loader mode before start C2PROG
-
The SCIA hardware connections are correct and working fine
-
When my code is running the SCIA is able to talk with a proprietary Windows App at 115200 bauds.
-
MCU is configured to use internal oscillator. (There is no crystal oscillator in the board)
-
The C2PROG has the correct COM PORT selected
-
The C2PROG is able to program the MCU when it is configured to use JTAG
-
I scope the GPIO28 during the connecting attempt and it seems the signal is correct, as you can see down below.
-
I also scope GPIO29 and as soon as the MCU enters in boot loader mode, the GPIO29 goes low and remain low. (I don't know why !)