This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-HC-C2-KIT: Technical issue

Part Number: DRV8301-HC-C2-KIT

Hi Team,

Our customer is using DRV8301-HC-C2-KIT evaluation module. Can you please help us regarding his concern?

Questions for TI.pdf

Regards,

Danilo

  • 1. Which is correct and can SPI-B be set up at the same time?

    No. These GPIOs must be configured for hall input if you need to connect the hall sensor. If the user doesn't need the hall sensor connection, these GPIOs can be configured to SPI-B. The GPIO24/25/26 are used for hall sensor input in the example project.

    2. Should we be able to see the signal hall-gpio-bitA, -B & -C?

    Yes. Rotate the motor by hand, the output signals of the Hall sensor can be monitored by using an oscilliscope. 

    3. What can we do about this?

    Please make sure that the target configuration file is set correctly with the right device.