Hello,
We are using TMS320F28069 to control a sensorless bldc motor; The motor is working great in torque mode however we are having some issues in speed mode where the motor keeps oscillating when we change the load. We have spent so much time tuning the speed loop but didn't help much. The application's for drones! The motor needs to ramp to 1200 rpm and keeps the speed at 1000 rpm as we change the load. The acceptable rpm variations is within 50 rpm. The motor is rated at 1200 rpm, 42V nominal. Appreciate your URGENT support.
Thanks