Part Number: TMDSCNCD28379D
I moved from 28335 to 28379D and I am trying to enable external mode. I am using TMDSDOCK28379D and Matlab R2018a and when trying to run External mode I get the following error message:
I am connected to the PC via USB cable to A:J1 on the controlCARD and the docking station is powered from a 5V supply on J1.
On the Matlab Answers site majority of the questions and answers are for LaunchPad F28379D, but even if I do the recommendations (change Rx/Tx GPIOs from 29/28 to 42/43 and set oscillator frequency to 10 MHz), it still does not work.
When selecting External mode and pressing the Run button I can (1) Load the application code to the controlCard (I see the signals on the scope) but (2) I cannot get into External mode. Boude rate is the same for COM port and Simulink.