This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM320F28335-HT: ADC external biasing components

Part Number: SM320F28335-HT


Hello,

I have a question regarding the 2.2uF caps that the data sheet says to add on the ADCREFx pins.  What effect would using a 1uF cap on these pins have on the ADC readings/functionality, specifically when operating at 200°C.  

Thanks,

Brandon

  • Brandon,

    The capacitors are relied upon to filter out voltage reference noise so I would expect that a smaller cap value might degrade the ADC accuracy to a certain extent. We don't have a practical way of modeling the exact effects. This tendency to degrade would apply at any operating temperature. I would not expect the ADC control logic / state machine to be affected.

    -Tommy