Part Number: TMS320F28379D
Greetings,
When initializing ePWM modules, I see in the example (from C2000) that we need to disable the pull-up resistors as below:
void InitEPwm3Gpio(void)
{
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO4 = 1; // Disable pull-up on GPIO4 (EPWM3A)
GpioCtrlRegs.GPAPUD.bit.GPIO5 = 1; // Disable pull-up on GPIO5 (EPWM3B)
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // Configure GPIO4 as EPWM3A
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // Configure GPIO5 as EPWM3B
EDIS;
}
Why do we need to do this? In which case, we need to enable those pull-up resistors?
Thanks.