Part Number: TMS320F28334
Other Parts Discussed in Thread: C2000WARE
Hello Guys,
Good day.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28334
Other Parts Discussed in Thread: C2000WARE
Hello Guys,
Good day.
Hi Art,
Is the piece of software intended for updating the firmware/application? There is no such code which programs the flash memory via USB. However, there are a couple of examples that can be used for reference . These are included in C2000Ware "f28335_can_flash_kernel" and "f28335_flash_kernel" (SCI) . These examples download code to RAM and then runs this code which allows application to be programmed into flash.
Best Regards
Siddharth
Thanks for looking into this Siddharth!
The customer wasn’t really looking for a new project to tackle.
He is just going to load CCS 3.3 on their panel PC with no source code.
Then their own customer can connect via the USB port and use the F28xx On-chip Flash Programmer to flash the chip.
Regards,
Art
Hi Art ,
Is the customer expecting to launch CCS and use the F28xx On-chip Flash Programmer ? If so, the board will need to have an onboard emulator to connect to the target
Best Regards
Siddharth
Hello Siddharth,
Good day.
The customer just realize that the docking station is equipped with an emulator. The only ic chip on this board capable of this function, he believe, is the FT2232D USB interface. Customer have incorporated this same circuitry into the board he is designing. Please let me know if the customer is missing something here.
Thanks and regards,
Art
Hi Art,
If the docking station has an emulator, can the customer connect the board to the docking station and use CCS to connect to the target? If so, then the On-chip flash programmer can be used.
Best Regards
Siddharth
Hello Siddharth,
Just a follow-up from the customer below in verbatim.
"I have built a prototype board, but I have not been able to connect to the processor with CCS 3.3.
I see in the docking station schematic that there is a chip labeled U3, which is a EEPROM.
Does this chip contain information or programming code necessary for the on-board emulator?
If so, is a programmed version available for integration into our custom board?"
Thanks and regards,
Art
Hi Art,
You can request the customer to have a look at the schematic of Control Card. This will give them an idea on how to interface an emulator
https://www.ti.com/lit/zip/sprr102
Best Regards
Siddharth