Part Number: TMS320F28379D
Hi,
Have a good day!
One customer suffer one issue when simulate through Matlab. This issue see as below:
I am using Matlab simulate DSP tms320f28379d. I gave a pulsed source to a gpio pin. the frequency was 1MHz. I also checked for 0.1MHz. Each time the output result was same almost half the frequency. I also want to know can I adjust the clocking from configuration parameters. If I can could you elaborately explain how each part like internal oscillator, prescaler, etc affects the output frequency valu.
If have any unclear about this issue pls, let me know.
Thanks and Best Regards
Jian, Sure