Other Parts Discussed in Thread: CCSTUDIO
I'm using the kit above as my final year project, and I'm experiencing some problems with the exercise given in the Renewable.pdf.
Firstly everything in Renewable.pdf is in the environment of CCStudio v3.3, and i'm using CCS v4; the control card assumed is TMS320F2803*,
while in actuality F2808 controlCard is provided with the kit.
My questions are as follows:
What build configuration should i select as active, F2803*RAM or F280*RAM? what about configurations ending with .flash, what's the difference?
As mentioned in the file, more advanced control can be implemented with this kit, for example, MPPT algorithm, I wonder if you can provided any places where I can find useful coding information about this?
In step23, when it says ''set start = 1.'', does it mean I can change the value in the watch window, will it immediately affect the running of the code, or should i change the value in the main.c file? also my resulting graphs definitely don't look like the ones in the file...
Thank you for your time!