This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28335: Help me sir, How to resolve this problem #10247-D null: creating output section "dcl32funcs" without a SECTIONS specification directform one controller C/C++ Problem

Part Number: TMDSCNCD28335


Respected Sir/Madam

My program is completely run but and the end it creates a warning which I showed below. So please help me with how to resolve it.

  • Hi Virendra,

    This means the application has a section named dcl32funcs which is not mapped to any memory blocks in the linker command file. Please update the linker command file to include the section mapping.

    dcl32funcs : > Flash region/RAM region

    If this is not specified in the linker command file, the section will allocated to the first available memory address.

    Regards,

    Veena