This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Matlab for C2000 micro controller.

Genius 9880 points

Part Number: TMS320F28388D

Hi Team, 

Customer want to confirm regarding our C2000 microcontroller. Below is the inquiry.

"Is it possible to configure multiple timers with different interrupts(Triggers) in C2000 with the Embedded Coder support package for C2000 Micro Controller in Matlab-Simulink.
Our Current understanding about the working is that, there will be a master timer (Discrete/Continuous Solver) which will be used to trigger different timers.


Our question is if multiple master timers can be configured in Simulink model using C2000 Package."

Thank you in advance.

Regards,

Maynard

  • Hi Maynard,

    From C2000 microcontroller perspective you can configure multiple timer interrupts, but I am not familiar with the Simulink model.

    Can you post this question on Mathworks forum, somebody in their team should be able to help you with Simulink model integration using C2000 Package.

    Best Regards,

    Nirav