This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: What is "ADCCTL1.RESET bit" in technical reference manual ?

Part Number: TMS320F28388D

Hi,

In spruii0c_F2838xD document, 

Table 20-25. ADCSOCPRICTL Register Field Descriptions

describes "when the ADCCTL1.RESET bit is set, or" like below.

However there is not any bits in 20.14.2.1 ADCCTL1 Register (Offset = 0h) [Reset = 0h]

Could le us know what is the correct specification ?

Best regards,

Hidehiko