Part Number: TMS320F28069
Hi TI expert
I am using tms320f28069 can bus to send data after receiving interference and meet several issues:
1. Is the CAN bus sending closed after the transmit error counter has accumulated to 255?
2. After can bus closed, whether it will effect receiving data or not?
3. When will the bus automatically return to normal? Is the transmit error counter cleared directly from 255 to 0? Or slowly decrease to 0 ?
4. The data cannot be sent after bus sending is turned off. It is not possible to judge whether the transmission is successful, and the counter value of transmit error counter cannot be reduced. Always 255?
Best regards,
Thomas