Part Number: TMS320F28386S
As I asked in the previous question, I wanted to implement the XDS onboard.
TI's replay was that this should work with no issues.
Now I have the new board with the SDX and here is the error I get:
Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 9.3.0.00042)
My guess is that the problem is that the EEPROM is blank.
How can I solve this?
Thanks!