Part Number: TMS320F280025C
Other Parts Discussed in Thread: LAUNCHXL-F280025C, C2000WARE
Hello experts,
I uses following CCS version on LAUNCHXL-F280025C , also uses C2000-CGT-21 compiler version.
Code Composer Studio Version: 10.3.0.00007
OS: Windows 10, v.10.0, x86_64 / win32 Java version: 1.8.0_144
WHen I tried to import the "C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f28002x\examples\hrcap" HRCAP sample program,
I found the following error message "Import failed for project 'hrcap' because its meta-data cannot be interpreted. Please contact support.".,
On the other hand , I could import the other project , for example, hrpwm_ex2_slider correctly.
Here my quesitons is, , why I can not import HRCAP sample project?
Regards, A.Fujinaka