This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335 and C++ standard library (STL)

Hi,

I am wondering if I can use C++ standard library functions in my code. For example, I would like to use "vector", for example,

test_stl.cpp

-------------------------------------------

#include "DSP28x_Project.h"  

#include <vector>

using namespace std;

int main()

{

     vector<int> a;

}

----------------------------------------------

It looks like it compiles. However, the linker complains

warning: creating output section ".cio" without a SECTIONS specification

"C:\\tidcs\\c28\\DSP2833x\\v131\\DSP2833x_common\\cmd\\28335_RAM_lnk.cmd", line 125: error: 

   placement fails for object ".text", size 0x1dfb (page 0).  Available ranges:

   RAML1        size: 0x1000       unused: 0x1000       max hole: 0x1000    

 

It looks like the memory is not enough to fit in the program. However, I just declare one vector variable. I am just wondering if this is normal. 

I am using ccs v3.3, by the way. 

Thanks a lot!!