Part Number: TMS320F28374D
HI everybody
I am trying to remove the following linker warning. It seems that it has enough heap memory, but why it generates that warning message?
warning #10210-D: creating ".esysmem" section with default size of 0x400; use the -heap option to change the default size
The map file shows like below.
.esysmem 1 00013000 00000400 UNINITIALIZED
00013000 00000004 rts2800_fpu32.lib : memory.c.obj (.esysmem)
00013004 000003fc --HOLE—
And below is from my linker file.
RAMGS7 : origin = 0x013000, length = 0x001000
.esysmem : > RAMGS7, PAGE = 1
what shoudl I do ?
thank you
BR
Carlo