Part Number: TMS320F28377D

1 I want SCI-boot1 when Boot mode =1 and FLASH-boot when Boot mode =3
2 I assume that Boot mode=3 ->get mode, Key!=0x5A -> flash boot
and Boot mode=1 ->sciboot ,BMODE=0x81 ->sci boot1
Is my assume right?
but after I program Z2-BOOTCTRL to 0x000081FF with CCS->tools->on chip flash ->PROGRAM Z2 OTPBOOTCTRL , The result is that the DSP will FLASH boot when BOOT mode =3 but SCI boot0 when boot mode =1, I can deliver the code by GPIO84 and GPIO85 , but cant deliver the CODE by GPIO28 and IO29.
Is the SCIBOOT (when Boot pin =1) only support SCI boot0?
If I set the key=0x5A, as I tested, I can successfully SCIBOOT1, but the DSP will always perform sci-boot1, no matter the Boot pin =1 or 3.