Part Number: TMS320F280049C
Hello TI-Team,
when compiling, my *.out files differ. The hex files are the same.
When comparing the files, I e.g. found out that in:
...
.data.2 {DFA30BC9-B2C9-4578-92EB-BBBFE2E95F80} SysCtl_getResetCause $C$L1 $C$L2 SysCtl_clearResetCause CPUTimer_stopTimer CPUTimer_startTimer $C$L3 $C$L4 $C$L5 $C$L6 $C$L7 $C$L8 $C$L9 $C$L10 $C$L11 $C$L12 $C$L13 $C$L14 $C$L15 $C$L16 $C$L17 $C$FSL1 $C$FSL2 $C$FSL3 $C$FSL4 $C$FSL5 $C$FSL6 $C$FSL7 .const:.string {A58CB782-A898-4600-ADAC-DEA38D321297} {639B9A42-AFF6-4819-B557-FC5C80EF991C} {59A6D344-53A1-4646-9F43-C92C509B9853}
...
{A58CB782-A898-4600-ADAC-DEA38D321297} these numbers differ. They are generated in .obj files/ .out file. I build release. Using the strip tool kept these numbers. What do they stand for, how can I get ride of them? Or more precise: How can I assure, that building on two different computers at two different point of times the generated *.out files are the same?
I am using the c2000 20.2.1 LTS compiler with eabi output format.
Thanks in advance.