Part Number: TMS320F28065
Team,
Table 7.13.1.1 of the datasheet SPRS698I says that the max ADC clock Freq is 45Mhz.
I assume that even if the TRM does not specify a max and suggest that high freq are possible, it is the datasheet that is providing a defiinitve answer for the max ADC clk freq that we specify for F2806x. The device must be used within the limits specified in the datasheet.
But trying to understand more on what is limiting the max ADC clock and what are the consequences:
-What are the factors that limits the max frequency?
-What kind of effect will be seen if we use the frequency above the max specified?
-What kind of effect will be seen if we use the frequency permanently above the max specified? Does it affects precision on the conversion? or will the ADC Fail to work properly?
I checked for Gen 3 devices and it seems that the max we specify for almost all the devices is 50 Mhz.
Thanks in advance!
A.