Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Routine name:
boot_ex1_cpu1_cpu2_cm_secure_flash_cpu1.c
Routine path:
C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2838x\examples\c28x\boot
problem:
I would like to ask whether the above routine is a routine that corresponds to the 0 pin of 28388D (as shown in the figure below) to FLASH.
According to this routine, it can be realized, in the case of no hardware circuit boot option, it can be modified by software, so that after power-on, the program can automatically run the program from FLASH. (The board in my hand has a problem. After power on, you must press the reset button to run the program.)