Part Number: TMS320F28069M
Hi everyone!

is there any thing else that I need to know for making such a kind of program & emulator?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28069M
Hi everyone!

Dave,
You are correct that the EEPROM needs an image. I've attached the files(along with a batch file) that should program the FTDI EEPROM to use as XDS100v2 with serial back channel.
Best,
Matthew3731.xds100v2-FT_Prog_v2.2.zip
thanks dear .
I am have another Home made programmer base on XDS100v1 which I took it from HVKit.v2.1(yellow PCB)
it is used FT2232D along with 93lc46 would you please tell me how to program FT2232D & 93lc46 thanks for your help
Best.
Dave.
One more question:
how can I program it ,is that via USB Cable that directly connected to FT2232D ,or any other Interface is need it?
I saw in some comment that said CPLD need it ?
would you please take a time and explain for me thanks.
Best.
Dave.
Dave,
This thread gives directions on programming for XDS100v1 https://e2e.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/21086/important----c2000-experimenter-kit-dual-rs232-fix
Yes, these can all be done via the same USB connection you have listed in your schematic. I think the link above will explain this a bit more completely for both cases(the XDS100v2 batch method is a bit less involved).
Best,
Matthew