This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: CLB SysConfig Errors when adding new CLB project to existing C++ project

Part Number: TMS320F28379D

Hi,

I'm working on a project where we need to use 4 eQEP modules for different quadrature encoders. In order to be able to read the 4th encoder, I created a CLB project using the necessary steps as stated in CLB Tool User's Guide (Rev. A) (ti.com) to act as the 4th eQEP. This program is working 100%. The problem occurs when I try to add this project to my existing C++ project. 

When I add the syscfg file and follow the steps in Chapter 6 (Enabling CLB Tool In Existing DriverLib Projects) the build log states "Device not found: F28X7X". I then add the device to the project properties, but after this when I build again, it finds "16 errors detected in the compilation of "syscfg/clb_config.c"". I'll attach all the relevant Build logs and problem snippets.

I'm currently using CCS9.3, because we are a few people working on different projects and want to use the same versions. However, I have installed CCS10.3 and the same errors occur as stated above.

My compiler version is: TI v20.2.2.LTS.

Any help will be greatly appreciated.

Kind regards,

Juan 


**** Build of configuration BUILD_FLASH for project VNLL Zoom Controller ****

"C:\\ti\\ccs930\\ccs\\utils\\bin\\gmake" -k -j 12 all -O 
 
Building file: "../clb_setup.syscfg"
Invoking: SysConfig
"C:/ti/ccs930/ccs/utils/sysconfig/sysconfig_cli.bat" -s "C:/ti/c2000/C2000Ware_3_04_00_00/utilities/clb_tool/clb_syscfg/.metadata/product.json" -o "syscfg" "../clb_setup.syscfg"
 
Usage:
 cli [-o <dir>] [-s <file>] [-u <string>] [-b <name>] [-d <name>] [-p <name>] [-r <name>] [--treatWarningsAsErrors] <script>
 cli --help
 cli --version
 
 example: cli -s meta_data/sdk.json -d MSP432P401R scripts/two_uarts.js
 example: -s sdk.json -d MSP432P401R -o ./display_cfg sdk/cfgs/display.syscfg
 
 Note that the all arguments other than '--help' and '--version' may also be 
 specified via the script with an embedded @cliArgs comment directive. 
 E.g. // @cliArgs -d MSP432P401R
 
 If an argument is embedded in a script and explicitly specified via the CLI
 then precedence is given to the CLI arguments. Additionally, specifying 
 "--board" or "--device" on the CLI will override any "--board" and "--device"
  arguments specified in the script.
 
subdir_rules.mk:12: recipe for target 'build-1573666367-inproc' failed
Device not found : F28X7X
gmake[1]: *** [build-1573666367-inproc] Error 1
subdir_rules.mk:9: recipe for target 'build-1573666367' failed
gmake: *** [build-1573666367] Error 2
gmake: Target 'all' not remade because of errors.

**** Build Finished ****
  Buildlog1.txt