Part Number: TMS320F280041
Other Parts Discussed in Thread: TMS320F28054
Currently, we use the TMS320F28054FPNT in our design, and we noticed that some PCB’s had some vibration/oscillation in the motor torque.
This small vibration was found to be caused by the control loop but originated in the ADC measurements on the phase voltages.
Each phase is sampled through a voltage divider from the Bus Voltage via a 150k and 4.70k 1% resistor divider string, with a 100nF capacitor, 5%, directly on the ADC input.
We changed the 1% resistors to 0.1% types and this almost solved the issue.
The used ADC inputs are : ADCINA7, ADCINB3, ADCINB0 (Used because we don't want the PGA in the design)
We noticed that one of the ADC inputs, ADCINB0, had a different leakage current then the other 2. (also on other boards)
The other 2 where exactly the same, (I measured 0.00xxx mV between these other two inputs) but +/-2 mV from ADCINB0 to either of the other 2.
Yes, in the datasheet is stated that there can be +/- 2uA leakage current on these pins.
I would like to know why is there a difference.
We plan to use the TMS320F280041CPZS on our next design, What re the leakage currents on the ADC input pins for the F280041?
Can I assume the same input specifications on the ADC input pins and use the same resistor-divider structure / leakage currents?
Thanks!