This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: HEX2000 question

Part Number: TMS320F280049


Hi Champ,

I want to know the HEX2000 under C2800 Compiler Tools v20.2.2.LTS folder  can working  on WIN7 32bit OS or not?

  • Unfortunately, no.  Starting with version 18.12.0.LTS, Windows executables of the C2000 compiler tools (which includes hex2000) are 64-bit executables.  Such executables do not work when run under any 32-bit Windows OS.

    Thanks and regards,

    -George