Part Number: TMS320F280049C
Hi All,
we have some problems regarding the use of the FAST estimator and I can only find an older documentation for FAST at http://www.ti.com/lit/ug/spruhj1h/spruhj1h.pdf .
Just as an example the document states the following prototype for the EST_run() function:
extern void EST_run(EST_Handle handle, const MATH_vec2 *pIab_pu, const MATH_vec2 *pVab_pu, const _iq dcBus_pu, const _iq speed_ref_pu);
On the other hand in the motor control SDK the prototype is:
extern void EST_run(EST_Handle handle, const EST_InputData_t *pInputData, EST_OutputData_t *pOutputData);
Is there a more current version of the document available?
Best regards,
Wolfgang