Part Number: TMS320F28069M
Other Parts Discussed in Thread: SYSBIOS
I setup the parameters of the eCAP as follows
void InitECapture()
{
InitECap1Gpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
ECap1Regs.ECEINT.all = 0x0000; // Disable all capture interrupts
ECap1Regs.ECCLR.all = 0xFFFF; // Clear all CAP interrupt flags
ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disable CAP1-CAP4 register loads
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Make sure the counter is stopped
// Configure peripheral registers
ECap1Regs.ECCTL2.bit.CONT_ONESHT = 1; // One-shot
ECap1Regs.ECCTL2.bit.STOP_WRAP = 3; // Stop at 4 events
ECap1Regs.ECCTL1.bit.CAP1POL = 1; // Falling edge
ECap1Regs.ECCTL1.bit.CAP2POL = 0; // Rising edge
ECap1Regs.ECCTL1.bit.CAP3POL = 1; // Falling edge
ECap1Regs.ECCTL1.bit.CAP4POL = 0; // Rising edge
ECap1Regs.ECCTL1.bit.CTRRST1 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST2 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST3 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST4 = 1; // Difference operation
ECap1Regs.ECCTL2.bit.SYNCI_EN = 1; // Enable sync in
ECap1Regs.ECCTL2.bit.SYNCO_SEL = 0; // Pass through
ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable capture units
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1; // Start Counter
ECap1Regs.ECCTL2.bit.REARM = 1; // arm one-shot
ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable CAP1-CAP4 register loads
ECap1Regs.ECEINT.bit.CEVT4 = 1; // 4 events = interrupt
// Enable CPU INT4 which is connected to ECAP1-4 INT:
IER |= M_INT4;
// Enable eCAP INTn in the PIE: Group 3 interrupt 1-6
PieCtrlRegs.PIEIER4.bit.INTx1 = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
}
And assigned the interrupt function in RTOS as follows:

However, the interrupt function doesn't seem to get called when running the code with a 1Hz signal attached to it. I am using GPIO24 (J6-pin55) as the pin to capture the signal. What am I missing?