Hi, I'm working with the 2808 development kit and I'm trying to get the CANa to receive. The code is below. It gets stuck on the do/while loop waiting for CANRMP to change. // TI File $Revision: /main/2 $ // Checkin $Date: July 31, 2009 14:26:08 $ //########################################################################### // Filename: Example_28xEcan_A_to_B_Xmit.c // // Description: eCAN-A To eCAN-B TXLOOP - Transmit loop // // ASSUMPTIONS: // // This program requires the DSP280x header files. // // Both CAN ports of the 280x DSP need to be connected // to each other (via CAN transceivers) // // eCANA is on GPIO31 (CANTXA) and // GPIO30 (CANRXA) // // eCANB is on GPIO8 (CANTXB) and // GPIO10 (CANRXB) // // As supplied, this project is configured for "boot to SARAM" // operation. The 280x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // Boot GPIO18 GPIO29 GPIO34 // Mode SPICLKA SCITXDA // SCITXB // ------------------------------------- // Flash 1 1 1 // SCI-A 1 1 0 // SPI-A 1 0 1 // I2C-A 1 0 0 // ECAN-A 0 1 1 // SARAM 0 1 0 <- "boot to SARAM" // OTP 0 0 1 // I/0 0 0 0 // // // DESCRIPTION: // // This example TRANSMITS data to another CAN module using MAILBOX5 // This program could either loop forever or transmit "n" # of times, // where "n" is the TXCOUNT value. // // This example can be used to check CAN-A and CAN-B. Since CAN-B is // initialized in DSP280x_ECan.c, it will acknowledge all frames // transmitted by the node on which this code runs. Both CAN ports of // the 280x DSP need to be connected to each other (via CAN transceivers) // //########################################################################### // Original Author: HJ // // $TI Release: DSP280x C/C++ Header Files V1.70 $ // $Release Date: July 27, 2009 $ //########################################################################### #include #include #define // Globals for this example long long void { Uint32 mdl; Uint32 mdh; /* Create a shadow register structure for the CAN control registers. This is needed, since, only 32-bit access is allowed to these registers. 16-bit access to these registers could potentially corrupt the register contents. This is especially true while writing to a bit (or group of bits) among bits 16 - 31 */ struct ECAN_REGS ECanaShadow;
// Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP280x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP280x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Just initalize eCAN pins for this example // This function is in DSP280x_ECan.c InitECanGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP280x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP280x_DefaultIsr.c. // This function is found in DSP280x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // No interrupts used in this example. // Step 4. Initialize all the Device Peripherals: // This function is found in DSP280x_InitPeripherals.c // InitPeripherals(); // Not required for this example // In this case just initalize eCAN-A and eCAN-B // This function is in DSP280x_ECan.c InitECan(); // Step 5. User specific code: /* Write to the MSGID field */ // ECanaMboxes.MBOX15.MSGID.all = 0x95555555; // Extended Identifier ECanaMboxes.MBOX25.MSGID.all = 0x81800000; //Standard Identifier - Transmit MBOX 15 ECanaMboxes.MBOX3.MSGID.all = 0xC200; // Standard Identifier - Rcv MBOX 3 /* Configure Mailbox under test as a Transmit mailbox */ ECanaShadow.CANMD.all = ECanaRegs.CANMD.all; ECanaShadow.CANMD.bit.MD15 = 0; ECanaShadow.CANMD.bit.MD3 = 1; ECanaRegs.CANMD.all = ECanaShadow.CANMD.all; /* Enable Mailbox under test */ ECanaShadow.CANME.all = ECanaRegs.CANME.all; ECanaShadow.CANME.bit.ME15 = 1; ECanaShadow.CANME.bit.ME3 = 1; ECanaRegs.CANME.all = ECanaShadow.CANME.all; /* Write to DLC field in Master Control reg */ ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 4; /* Clear to the transmit mailbox RAM field */ ECanaMboxes.MBOX15.MDL.all = 0x00000000; ECanaMboxes.MBOX15.MDH.all = 0x00000000; /* Begin reading from receive mailbox 3 */ ECanaShadow.CANRMP.bit.RMP3 = 0; ECanaRegs.CANRMP.all = ECanaShadow.CANRMP.all; mdl=0; mdh=0; do
{ ECanaShadow.CANRMP.all = ECanaRegs.CANRMP.all; } while(ECanaShadow.CANRMP.bit.RMP3 == 0); // Wait for CANRMP bit to be set.. ECanaRegs.CANRMP.bit.RMP3 = 1; mdl = ECanaMboxes.MBOX3.MDL.all; mdh = ECanaMboxes.MBOX3.MDH.all; /* Copy received data to the transmit mailbox RAM field */ ECanaMboxes.MBOX15.MDL.all = mdl; ECanaMboxes.MBOX15.MDH.all = mdh; ECanaRegs.CANRMP.bit.RMP3 = 0; /* Begin transmitting */ for(i=0; i < TXCOUNT; i++)
{ ECanaShadow.CANTRS.all = 0; ECanaShadow.CANTRS.bit.TRS15 = 1; // Set TRS for mailbox under test ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all; do
{ ECanaShadow.CANTA.all = ECanaRegs.CANTA.all; } while(ECanaShadow.CANTA.bit.TA15 == 0 );
ECanaShadow.CANTA.all = 0; ECanaShadow.CANTA.bit.TA15 = 1; // Clear TA5 ECanaRegs.CANTA.all = ECanaShadow.CANTA.all; loopcount ++; } asm(" ESTOP0"); // Stop here }