Hi,
When checking the circuit diagram of Launchxl-F280049C, can I think that TMC and TCK can be written by connecting GND to XDS110?
Is it okay to recognize that TRST is not needed to write a program?
Koki

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When checking the circuit diagram of Launchxl-F280049C, can I think that TMC and TCK can be written by connecting GND to XDS110?
Is it okay to recognize that TRST is not needed to write a program?
Koki

Hi Koki,
Can you clarify your question? I don't quite understand what you're asking.
TMS and TCK connections between the XDS110 (MSP432) and F280049C device are needed for 2-pin C-JTAG programming/debugging of the F280049C. The F280049C device does not have a TRST pin.
Best,
Kevin