Part Number: TMDSCNCD28035
Other Parts Discussed in Thread: TMDSDOCK28035, , C2000WARE
While running a program on the Piccolo f28035, I had an error show up saying that the processor was in low power mode. I replied to all the options in the pop-up, but it would not clear. I hit the cancel button and hit CTRL-F2 and Composer Studio froze. I killed the process, then restarted. After cleaning the project and recompiling, started the debugger. The following error has appeared and with a load error.
C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.3.0.00042)
Would you advise me on how to take the device out of reset?
Dan O'Connor
303-827-4117
dan@renewpower.us
error. It is possible that I could have taxed the power output of the board. It is hard believe, since I was running an inductor in series with a capacitor to ground. I'm running the board through TMDSDOCK28035, the TI Docking-Stn USB-EMU [R3] TXN100. I'll go ahead and do the testing you suggested and get back to you. Thanks, Dan