Part Number: TMS320F28335
Hello,
I am programming a TMS320F28335 and right now I have some connectivity issues with the MCU. The MCU is part of the experimental development kit provided by TI.
When I am trying to deploy the code on the board through the USB port (either in CCS or Embedded Coder), I get the following error:
C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.3.0.00032)
Also, the MCU overheats quickly once I plug in the USB cable - too hot to touch it after few seconds.
Notes:
- Jumper in J9 connected and the JTAG DR Integrity scan-test has succeeded.
- The 5 V and 3.3 V pins on the docking station have the correct potential.
- The LD1 on the control board dims lightly - not bright as the power led on the docking station. The Vout_1 of U2 component on the control board is 2.4 V instead of 3.3 V (I measured the voltage on L19). The Vout_2 of U2 component seems to be correct - the voltage measured on L20 is 1.8 V.
- All boot pins GPIOs 84-87 are on ON position.
- SW1 is in OFF position.
Any idea what the problem can be?
thanks
Fra