Part Number: TMS320F28377D-Q1
Other Parts Discussed in Thread: TMS320F2811
When doing a calibration on the TMS320F28377 while using an external VREF, is it assumed that the calibration signal applied to the ADC input is a maximum signal equal to the external VREF? With this assumption it appears from the documentation that only an offset correction is obtained. What would happen if the signal applied to the ADC input is not a maximum signal, but something like 50% to 80% of the maximum signal of VREF? Would the calibration also produce a gain correction that would cause all signals converted afterward to read higher than normal by the inverse ratio of the calibration signal to the maximum signal? (I realize that the calibration signal should be a regulated voltage like the VREF voltage, but a circuit I am analyzing has used a non-regulated signal instead).
Related question: Do the same answers apply to the TMS320F2811 DSP?