Part Number: TMS320F28069
We are using PICCOLO std control card. Our code can be loaded from CCS and run by selecting from RUN after loading to the device thru JTAG.
But if we load it to flash, it won't start executing the code from flash when we cold start from Power ON .
What are the exact steps to carry out in the code including adding .h files, .include files & linker files that will start code execution on powering the device?
In a manner of the old days, do we have to add any hardware such as pulling a particular pin that rises to VCC with a time constant that signals some internal block to start executing the program?
It is BTW an Inverter.
Any help will be highly appreciated.
r