Part Number: TMS320F28076
I developed the firmware with the CCS9.3; if I launch the firmware using the debug (the XDS110 probe connected) all works good. The problem starts when I add in code array of 1600 values (uint16_t array[1600]) and try to start working with it . I've load the firmware , power of the board and power on it again my firmware doesn't work. I checked when I add an array of 1500 values everything works fine.
I have created the same array (uint16_t array [1600]) in the project example (gpio_ex2_toogle) from Resource Explorer and the situation is the same. Firmware doesn't boot from flash after power reset.
I need your help...
Thank you